Hello,
I am planning to use TXB0104 to translate the signal level of SPI signals from 3.3V (from microprocessor) to 5V (for slave devices). There are 3 slave devices on the same SPI bus with different chip selects.
The slave devices are as below:
1. SPI based Isolator + Digital - Analog Converter
2. SPI based 8 channel Relay driver (TPL9202)
3. SPI based 8 channel solenoid driver (TPL9202)
Is the drive strength of TXB0104 enough to drive these devices or do I need to use a buffer after the translation ?
Please advise along with suggestions for translator if any.
Thanks,
Naveen