Hello community,
i have a SPI-Master with 1,8 high-level output voltage and a SPI-Slave with minimal 3,5 high-level input voltage. Can i use the SN74AVC4T774 level translater to connect these two devices?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello community,
i have a SPI-Master with 1,8 high-level output voltage and a SPI-Slave with minimal 3,5 high-level input voltage. Can i use the SN74AVC4T774 level translater to connect these two devices?
I have another question, just to make it clear... Unfortunately my SPI-Slave has at the SO-Pin a 4.5 high level output voltage. Can i use the SN74AVC4T774 with this voltage? I read something like the I/Os are 4.6 volt tolerant...
Franz,
Sorry I missed this. Yes, the IOs are 4.6V tolerant, so it will be able to handle a 4.5V input without damage.