What's the difference of the two package?
The application scenario is to perform level conversion of 1.8V-3.3V for 14 GPIO signals.
Which one performs better? Thanks.
Regards, Charlie
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What's the difference of the two package?
The application scenario is to perform level conversion of 1.8V-3.3V for 14 GPIO signals.
Which one performs better? Thanks.
Regards, Charlie
Hey Charlie,
To add on, the functionality will be the same across the different package types. Note that LSF0108 would work for GPIO signals but there are more suitable devices for your application such as direction controlled/fixed direction devices. See the below for more information:
Regards,
Jack