Part Number: SN74AVC16T245
Other Parts Discussed in Thread: DS90LV011A, DS15BR400, SN74AVC2T245, SN74LVC8T245, SN74LVC16T245, TXU0204, SN74LXC2T45
Hi,
I am going to tanslate a 200Mbps signal from 1.8V to 3.3V. The SN74AVC16T245 maximum data rate is 380Mbps for 1.8V to 3.3V level- shifting in the datasheet. but i aslo see the maximum tPLH and tPHL in switching caractersitics is 3.3ns. Does it mean the worst data rate is only 151Mbps (1/(3.3ns+3.3ns))? if i wish to tansfer the 200Mbps signal stably. what model may i use?
Regards,
Shu