Hi All,
The SN74LVC8T245 datasheet specifies that input circuitry for both ports A and B is always active and requires a logic level (high or low) to be applied. Does this mean
1. Pins at ports A and B cannot be left floating even when outputs are disabled OE = 1?
2. Are there example circuits for this chip, an application note etc.?
3. If current consumption does rise due to floating A and/or B ports will it revert to normal if valid logic levels are presented to the inputs? That is, is the high ICC, or ICCZ a temporary feature that does not require the SN74LVC8T245 to be power cycled in the event of high ICC or ICCZ?
Thanks!
Anand