Part Number: SN74LV1T34
Other Parts Discussed in Thread: SN74LVC2G34, , SN74LVC1G34
Hello,
A customer is asking if the SN74LV1T34DCKR could drive load of 30mA ?
Could you please advise?
Thanks,
VL
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74LV1T34
Other Parts Discussed in Thread: SN74LVC2G34, , SN74LVC1G34
Hello,
A customer is asking if the SN74LV1T34DCKR could drive load of 30mA ?
Could you please advise?
Thanks,
VL
The absolute maximum rating is 25 mA, so the device might get damaged.
And even exceeding the recommended operating condition (of 8 mA in this case) would probably not leave enough voltage for the load. Please note that the supply voltage affects the drive strength.
Use a logic family with stronger output drivers, and use multiple outputs in parallel, if needed. You probably want the SN74LVC2G34. (If the input signal has a lower voltage, put a level shifter like the SN74LV1T34 in front.)
Yes.
Even a single LVC output (e.g., SN74LVC1G34) is rated for 32 mA, but the VOL of 0.55 V leaves only 3.95 V for the load. You have to determine if that is enough for your application. (With two outputs, VOL is halved.)