Part Number: TXS0102
Other Parts Discussed in Thread: LSF0102
Hi
We are using TXS0102DQER in our design. Kindly suggest a equivalent alternate part for the same.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Premalatha,
The LSF0102 has the DQE package as well that supports both push-pull and open drain applications. Note that this device does not have internal pull up resistors like the TXS0102, so external pull up resistors may be required by the user. However, auto-bidirectional level shifters are generally used for auto-bidirectional signals that have information flowing to and from each channel. If your application does not have this, please refer to the direction controlled/fixed direction level shifters such as the TXU0x02 and the AXC2T45.
In order to give you a more accurate recommendation, more info is needed. What interface is being used during translation? What is the voltage shift/data rates that is needed in your application?
Regards,
Jack