Part Number: LSF0204
Other Parts Discussed in Thread: TXB0304
Hi,
Please kindly advise if the LSF0204 is available for Qual-SPI solution?
If yes, what is the max. frequency for LSF0204, thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Clemens,
You mean the TXB0304 is available for Qual-SPI, and LSF0204 isn't well?
The LSF can be used for Quad SPI, but if the devices do not have enough drive strength, or if the traces are too long, you might not be able to reach the desired speed.
The TXB is a buffered device, so its limits are less strict. See section 6.6 of the datasheet.