Part Number: SN74HCS74
Other Parts Discussed in Thread: SN74LVC1G00, SN74LVC1G132
Hi Logic Experts,
I'm using the sn74HCS74 to control power on/off. Below is my schematic.

The clock signal is drived by the output of the SN74LVC1G00。
Here is the problem I met:
The Q output is changed by both rising-edge and falling-edge clock signal !
The circuit works well after I replaced the SN74LVC1G00 with the SN74LVC1G132.
Apparently the problem caused by the clock signal.But I got confused! Why is that,since the SH74HCS74 inputs allow for slow or noisy input
signals?
Thanks!
Tyrael