This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About the Data Rate of SN74CBTLV3861

Other Parts Discussed in Thread: SN74CBTLV3861, SN74CB3T3383, SN74AVC8T245

In my current design,

I need to translator HDMI's LVCMOS33 Data output to LVCMOS25 for input of Virtex-6 FPGA.

I want to use SN74CBTLV3861 to serve as level convertor

But I don't know that what is the max data rate of SN74CBTLV3861

HDMI output clk's  frequency may be above 150MHz, 

so I wonder if SN74CBTLV3861 is OK for this application.

or are there other chip suitable to be 3.3V --> 2.5V 's level convertor??

 

Thank you !