This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD4060B: Automotive grade timer with similar features as CD-4060 with lesser number of output pins

Part Number: CD4060B


Hi,  

Do you have a automotive grade timer  for providing turn on duration from 5 seconds to 60 seconds and so on.

Regards

Shama

  • The only device with the same features as the CD4060B is the CD4060B. What features do you actually need?

    Do you have an external clock source, or a crystal, or an R-C circuit? How is the timer triggered? Is it required to be regtriggerable?

    (There is not any automotive counter or timer with fewer than 16 pins.)