This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is there any need for time delay for OE



Hello,

We are using TXS0104ED in our design. We wanted to know, if there is any need to provide a time delay of say 1us for the the outputs of the translator to be active after power ON.

For instance, VCCA = 1.8V and VCCB=3.3V. Then, at the time of power on, should we include an RC circuit to introduce a time delay (with one end of R tied to 1.8V) before the outputs get enabled for their operation.

Request your kind support at the earliest.

Thanks and Regards,

Vinay

  • The device should become operational close to 200ns after power on. However, the 'one-shot' edge acceleration circuitry takes about 1us to charge after being enabled/powered.

     

    I do not understand what you mean by introducing a time delay using an RC circuit. Without further understanding, my concern is that such a circuit would hurt device performance when under operation.

     

     

  • It is OK to tie OE directly to VCCA, although there will be the delay before the IOs are fully operational.