Part Number: LSF0102
Other Parts Discussed in Thread: TCA9800
Hello, I have some problem with the LSF0102DQE, while I'm using him as a I2C shifter from 1.2v to 3.3v.
I have a designed circuit :

Before my testing all the Rpu were 5K and the signal(after the shifter) were looked as :

After some "playing" with my RpaA and RpaB the best signal looks :

but still I can't see a prefect I2C bus, my HAC/NAC always changes not going back to 0 geting back to 0.44v , some bits during the switching between high to low not going back to 0v as well .
My I2C freq is not more than 400KHz, as in the spec (on 3.3v of I2c protocol ) the Rpu need to be between 320-2.9k, with this spec I tested the board but it was looking more like the first pic.
Am I doing something wrong ? what do i miss, or the LSF can't be a Buffer for I2C bus ?