Part Number: LSF0108
Other Parts Discussed in Thread: TXS0101
Hi Expert,
Customer are searching for a buffer IC, which need to be used on LPC IRQ signal.
This is bi-directional signal, can be output from CPU or from BMC.
Please kindly help to check if there is bidirectional buffer with 3.3V for our application.
If yes, please share the spec with use.
Regards,
Mark