Other Parts Discussed in Thread: PGA113, PGA113EVM-B, OPA364
Hi :
Can TI provide PGA113 Pspice model for reference ?
thx
Best Regards,
Arang
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: PGA113, PGA113EVM-B, OPA364
Hi :
Can TI provide PGA113 Pspice model for reference ?
thx
Best Regards,
Arang
Hi Arang,
The PGA113 was developed and introduced to the market over a decade ago and unfortunately no SPICE model was developed for this part. The best way to get familiar with this device is through our evaluation module PGA113EVM-B. I checked the inventory on ti.com and we do have this evaluation module in stock.
https://www.ti.com/tool/PGA113EVM-B
Regards,
Zach
Hi ,
I want to change my circuit to use PGA113,
original circuit as attached file,
could you help to provide reference design circuit to use PGA113 for my circuit ?
thx

Best Regards,
Arang
Hi Arang,
It looks like you are intending to use the PGA113 as a simple programmable gain block to replace the fixed-gain amplifier in your circuit. The PGA113 has some additional features such as an input multiplexer and internal calibration channels that can be used for system-level calibration. Are you looking for a reference design that includes the calibration or multiplexer features?
Figure 72 from the PGA113 datasheet shows a typical configuration using the calibration channels. Note that Vcal/CH0 must be connected to the ADC reference potential to use the calibration (in this figure it is connected to AVDD because this is equal to the ADC Ref voltage). The PGA113 VREF pin must be connected to a low-impedance reference capable of sourcing and sinking at least 2mA. Figure 72 shows the OPA364 in a buffer configuration to provide the low-impedance voltage to the VREF pin.

If you do not require the calibration feature you may use the configuration shown above and simply use the multiplexer to select CH1 as your input.
I see your input source is expected to be between 30mV and 500mV at 1550Hz but the schematic does not show what this is referenced to. Is this 30mV-500mV input signal referenced to ground? Or is it referenced to the 1.65V mid-supply?
What type of sensor is connected to the input? If this input signal is connected to the outside world you may need to include some protection circuitry in case of an electrical overstress event. This article provides helpful information on electrical overstress protection: https://www.ednasia.com/provide-robust-input-overvoltage-protection-for-amplifier-analog-input-modules/.
Regards,
Zach