Part Number: CD4017B
Other Parts Discussed in Thread: CD4514B, CD4510B, SN74HCS74, SN74HCS164
Hi Experts,
Our customer is looking for a schematic for the CD4017B cascade timer for 20 to 80 lights. He have a few circuits he got off the internet, but they allow 4 lights to be on at the same time running together.
It is a so-called chaser or sequencer is one of the most popular types of LED-driving circuit and is widely used in advertising displays and in running-light ‘rope’ displays in small discos, etc. Driven by a 555 timer and cascades the lights. The circuits he has found do not work properly.
I cannot find the data to show how to cascade the 4017 for multiple 4017s. He uses the 555 timer for Pulse Wave Modulation for motor speed control by adjusting the duty cycle and can set the circuit for an adjustable pulse rate to adjust the speed of the chaser.
He was hoping we would be able to simply give him the schematic he need. He said: is this too complicated of an issue for TI? Or should I just expect to only make chaser lights of 10 maximum?
I hope you can help us. Thank you.
Best regards,
Gerald