Other Parts Discussed in Thread: SN74LVC1G125,
Hi team,
In the datasheet, it says
"The device can produce 24 mA of drive current at 3.3 V, which is ideal for driving multiple outputs and good for high-speed applications up to 100 MHz"
I guess this means that when Vcc=3.3V, maximum signal speed is 100MHz and the device can drive 24mA in that condition, right?
Also, how about when Vcc=1.2V? What is the signal speed limitation for Vcc=1.2V?
Regards,
Ohashi