Other Parts Discussed in Thread: TLV840, SN74LVC1G123, TLV809E, TPS3700, TPS3899, TPS3703
Hi,
Im looking for device that create pulse Xms after power up without any external involvement. The picture below show's the operational i want.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
Do you want a sigle pulse or should it be pulse train ? I can see red and green waveforms ? can you please explain them.
Regards
Trailokya
Hi
i need single pulse. the output can be as the green line or as the red line
Hi
You can use below circuit -

TPS3700 + TPS3899

Let me know if you have any question.
Regards
Trailokya
can i make the trigger with resistor and capacitor ? im trying to minimize components.
maybe to use SN74LVC1G123, hold CLRn high, An low and make a RC delay for B to make the rise edge ?

hi Trailokya
I try to minimize components. If you know components that have an overvoltage detector (threshold 0.4-1.2V) and latched after this threshold is exceeded, that could help me.
You can use the '123 alone, if you can live with the RC delay not being very accurate.
thanks Clemens
If you know components that have an overvoltage detector (threshold 0.4-1.2V) and latched after this threshold is exceeded, that could help me also.
Hi Yoav
TPS3703 has latch feature where you can take the CT voltage below VCT and latch the reset.
You need to take the CT voltage above VCT with some RC. Also you need to slow downm your single pulse if you want to use only one IC. Please refer below app not https://www.ti.com/lit/an/snva836a/snva836a.pdf?ts=1672039096371&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct%252FTPS3820 for more details.
Regards
Trailokya