We would like to use the part in the following manner:
Va=1.8V with the option of using a 1.8V or 3.3V input
Vb would be 3.3V
Is this feasable.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yes; the A input is overvoltage tolerant. See [FAQ] Can the input voltage (Vi) to my logic device be higher than the supply voltage (Vcc)?