This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Looking for eSPI buffer



Dear team,

I am looking for eSPI bidirection buffer solutino. (Vcc 1.8V、Frequency 100MHz 、6 channel or 8 channel)

Did we have recommended solution for this application?

Regards,

Ben

  • There is no such device.

    Bidirectional buffering is possible only if there is a direction signal (see any SN74xxx245 transceiver or translator), or if the buffer knows the direction by decoding and understanding the protocol. Without a direction signal, it is not possible to determine if the voltage at pin A should override the voltage at pin B, or if the voltage at pin B should override the voltage at pin A.