This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN54SLC8T245-SEP: Min/Max propagation delay specifications?

Part Number: SN54SLC8T245-SEP


Hello,

I am wondering if there is info available on the min and max propagation delays from A to B and from B to A when VCCA = 1.5V for the cases where VCCA = 1.8V and VCCA = 3.3V. Only the typical is specified for both directions on the datasheet.

This info is useful for worst-case timing analysis. Any insight is appreciated.

  • Hi Jack,

    We usually spec typical propagation delay values per system variation. However, the best way to get min/max propagation delay specifications would be to prototype and test it out based on the use case.

    Hope this helps. Thanks!

    Best,

    Swathi