Hi,
We are using CD74HC04. There was no significant difference in the threshold values for both Lo→Hi and Hi→Lo for the normal products that had been used until now.
However, all newly delivered chips have a hysteresis of about 700mV. The input voltage when the output voltage changes from Lo to Hi is -549mV. Also, the input voltage when the output voltage changes from Hi to Lo is 138mV.
* Since the power supply to the product is ±2.5V, the Hi level is 2.5V and the Lo level is -2.5V.
Is this a spec according to the datasheet?
[The normal products]

[Chip with hysteresis]

Thanks,
Eevee