Part Number: LSF0102
Other Parts Discussed in Thread: CD4010B, CD40109B, LSF0108, LSF0101
Hi Team,
LSF is a bidirectional switching chip. I want to know, is the one-way chip cheaper?
My customer's demand is:
use a single-chip microcomputer to control the fan. The voltage of the microcontroller is 3.3V, and the voltage of the fan is 5V. It is necessary to convert the 3V level to the 5V level. A total of nine channels are required. The communication rate is not high, lower than LSF0102. Level shifting in one direction is sufficient.
Please recommend the level shifter with the best price. Thanks.
Regards,
Charlie