This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC126A-Q1: the orderable number is different where it is shown in datasheet and ti.com

Part Number: SN74LVC126A-Q1

Hi team,

      The customers want to use the SN74LVC126A-Q1, but the orderable number is different shown in datasheet and ti.com.

       In ti.com, the SN74LVC126A-Q1 in the package of TSSOP-14 is CLVC126AQPWRG4Q1 shown below.

      In the datasheet, the SN74LVC126A-Q1 in the package of TSSOP-14 is SN74LVC126AQPWRQ1 shown below.

      Could you please confirm which orderable number is right one to help customer to place orders?

      In addition, CLVC126AQPWRG4Q1 (package TSSOP-14) and SN74LVC126AQDRQ1 (package SOIC-14) ,these two materials are only different in package, right? So share a the same specification?

YOURS

NAN