Hi, I designed a board that interfaces with another existing board. The other board drives some logic signals with a MAX3002 level shifter. The new board also uses a level shifter TSX0108. Most signals are uni directional with the 0108 driving the 3002. But the 3002 drives one signal into the 0108 and every thing works fine. But during a elevated temperature test we disconverd that when the input to the 3002 is driven low the output follows, as it should but the output slowly drifts from 0 up to a value greater than the logic low threshold even though the 3002 input is held low. It looks capacitive, I have no pull up or pull down signals on the signals between the 3002 and 0108.
Any thoughts on this?
Steve