Hi,
We want to clarify two things from the TI application note.
1. The minimum transition rate, dt/dv of SN74LVC is 5/10 as per the table given below. Does this mean 5ns rise rate and 10ns fall rate? What does the minimum required transition rate mean? Does this mean that the input signal should not go faster than that, for eg, if the input clock transition rise rate is 1ns/V which is faster than 5ns/V, does this affect the functionality of the IC?

2. Regarding dt/dv calculation, as mentioned in the application note, it is better to define rise and fall times over the range between VIL(max) and VIH(min). Is it correct if the equation is modified as shown below: Please confirm.
Modified equation:

Regards
Sreelekshmi.