Other Parts Discussed in Thread: TXU0304, TXU0104, SN74LVC1G34
I got some SN74AVCH4T245DR IC samples recently
I wanted to use them for shifting level between 5V SPI and 1.8V SPI interface
It took a long time to select this IC, and it turned out it is 2x2 CH (2 direction controls are connected to 2-2 channels) so it not really fit in my application. Transmit direction: CS, CLK, MOSI (+ one extra 10MHz clock) receive direction: MISO
I don't know if you are more familiar with these level shifters, but would be great if you can suggest something that is simple and fitt in my application