Part Number: TXB0104
Other Parts Discussed in Thread: TXU0304, TXU0104, TXU0204, TXU0202, TXU0102, TXS0108E, TXS0104E, TXS0206, TXS0102, SN74AXC8T245, SN74AXC4T774, SN74AXC4T245
Hi
In one of our FPGA board designs, we have to use voltage converters to connect a few UARTs (RS-232 and RS-422 ) interfaces, as the FPGA bank voltages and external Transceiver voltages are not matching . We need a throughput of around 1Mbps (921 kbps) for these UARTs.
Ours is a very small form factor and low power design.
Some places we need 6 nets and few other 4 nets to be voltage converted. We were planning to consider TXB0104QPWRQ1, TXB0106PW for voltage conversions from 1.8V to 3.3V Can you confirm if these parts support 921kbps speed. Are there any better small form factor devices that are meant to be used as UART signals level converters at a speed of 921 kbps.
Regards
Binu