Other Parts Discussed in Thread: SN74LVC1G126
The parts are SN74AUP1G126DCKR.
Are there any chances that the following condition will continue to damage the parts?
This is when the 4pin of the output terminal and the power supply (3.3V) different from the power supply used by the SN74AUP1G126 are shorted.
6.1 Absolute Maximum Ratings in the datasheet states that Io Continuous output current is Max.20mA.
I'm worried about the parts being damaged when trying to output a current of 20mA or more due to a short circuit with the power supply.