Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G373: SN74LVC1G373YZPR

Part Number: SN74LVC1G373

SOM CARD_20230217_LA.pdfSN74LVC1G373 SCH review

  • This part of the schematic does not show a decoupling capacitor.

    With D connected to GND, the output can never be high, so RESET_D never has an effect. Only PMIC_EXT_EN_OUT_R switches the output between GND and Hi-Z.

    What is the purpose of this circuit? What effect should RESET_L have?

  • May I know which pin needs a decoupling capacitor., is VCC pin?

    We use these circuit as latch buffer, only PMIC_EXT_EN low, RESET low, the circuit output will closed carrier board power.

  • When power on, EXT_EN will be high, output will be high Z mode,

    When power off, RESET will be low, and EXT_EN will low,  out put will be low to shutdown my carrier board power

  • Hi Leo,

    May I know which pin needs a decoupling capacitor., is VCC pin?

    Yes, VCC for any logic device should have a 0.1uF bypass capacitor. From the datasheet:

    When power on, EXT_EN will be high, output will be high Z mode,

    When power off, RESET will be low, and EXT_EN will low,  out put will be low to shutdown my carrier board power

    I'm not sure this circuit will do what you expect. The Q output at power up (VCC_1V8_S3 turn on) is unknown - the latch does not have a known output state until it has been loaded with data.

    The signal RESET_D could only have an effect if Q happened to start in the high state, after which it would no longer have an effect as the latch would remain in the low state.

    The pull-up to VCC5V0_SYS will cause the output to go to 5V when Q is in the high-impedance state, however this won't set the latch state to high - as soon as the output is enabled again, it will be pulled back to 0V.

  • When system power on, we want shutdownreq keep high, shutdownreq was link to our carrier board 5V EN pin.

    When system power off, we want shutdownreq after EXT_EN change to low, shutdownreq output change to low state, to turn off 5V EN pin.

    EXT_EN this pin can show our PMIC IC state, EXT_EN high was system turn on, EXT_EN low was system turn off

    The Q output at power up (VCC_1V8_S3 turn on) is unknown -> my output has a PU RES, I think it will keep high, we expet only system turn off, this circuit will be active, and when EXT_EN change to low, output Q also change to low to shutdown my carrier board power en pin

  • The initial state of the latch is undefined; see [FAQ] What is the default output of a latched device? (Flip-Flop, latch, register) If the initial state of the latch happens to be low, then it will actively drive its output low, and the pull-up resistor will have no effect.

    The latch is powered by VCC_1V8_S3, so its output can go high only when VCC_1V8_S3 is powering up, and must go down when VCC_1V8_S3 is powering down. But the pull-up resistor to VCC5V0_SYS means that the output will be pulled high when the latch is powered down, so the SHUTDOWN_REQN_5V signal will go up and down when VCC5V0_SYS is powering up/down.

    Is VSYS_5V the same as VCC5V0_SYS?

    In your timing diagram, you have shown all edges at different times. But this is not possible; the SHUTDOWN_REQN_5V can change only when (at least) one of its inputs change, or when its power supply changes. Please specify exactly how the value of SHUTDOWN_REQN_5V is determined by the other four signals/supplies.