This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN54LS374: What are the specific differences between SN54LS374 and SNJ54LS374J?

Part Number: SN54LS374


What are the specific differences between SN54LS374 and SNJ54LS374J?  

  • Hello Xiaofu,

    "SN54LS374" is what we refer to as a Generic Part Number, or GPN. To give a full description:  SN is the prefix used for TI logic devices. 54 indicates a military rated device. LS is the logic family (Low-power Schottky), and 374 is the function (Octal D-type flip-flops).

    "SNJ54LS374J" is what we refer to as an Orderable Part number, or OPN. This provides a specific orderable part number, and this one in particular is for the "J" package, a ceramic dual-inline type package.

    Or, in other words, these are not different devices, but two ways to refer to the same device.