This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HC14: Question about the output capacitance, 70pF.

Part Number: SN74HC14


Hello guys,

One of my customers has the following question about SN74HC14 output capacitance.

Q. SN74HC14 datasheet says that "Ensure the capacitive load at the output is ≤ 70 pF. This is ...." in 9.2.2 Detailed Design Procedure section.
     If the capacitance is exceeded 70pF, what is happen? Why the output capacitance is need to be less than 70pF? 

Could you please give me your reply?

Your reply would be much appreciated.

Best regards,
Kazuya.