Part Number: TXB0302
Other Parts Discussed in Thread: TXS0102, LSF0102
Could you explain why TXB0302 can't use for open drain case?
Could you show me the fail case?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Weilun,
The TXB device series will not support open drain cases because there is a series resistor at the output that assists with the auto-direction sensing circuitry. For this same reason, we suggest that if external pullup resistors are to be used with this device, they must be >20kOhms to not contend with the output drivers of this device (hence not suitable for open drain use cases).

See the LSF0102 or the TXS0102 for level translation with open drain applications.
Regards,
Jack
Hey Weilun,
If a 9kohm pullup resistor was used, the VOH would not be impacted- but the VOL will become a voltage divider with the internal 1kohm and could contend with the output drivers of the TXB0302 since it fails to meet the requirement of >20Kohms.
If your application requires external pullup resistors on the I2C data line, I recommend taking a look at the TXS0102 (has internal 10k pullups that can be used so you would not need the 9kOhms).
Thanks,
Jack
Hey Weilun,
Using external pullups less than 20kohms with this device primarily impacts VOH and VOL- no other concern comes to my mind at the moment.
If you are satisfied with the open drain signals while using the 9kohms and on this device, then it is at your discretion. We just generally recommend TXS/ LSF devices for open drain signals.
Regards,
Jack