Part Number: SN74ABTH16245
Hello, I'm having trouble with this component in a high speed design (100Mbps - 200Mbps). It looks like this component is swallowing some bits at both these rates. Looking further into the datasheet, I see the minimum pulse duration is not specified, tw.
In the datasheet, the only specified parameters are the propagation delay times. What are the setup and hold times for this component alongside Tw? Is there a larger table for these component values available somewhere? The current documentation appears to be quite sparse compared to other logic components.
Thank you!