Other Parts Discussed in Thread: SN74LVC1G123
Hi expert,
I am attempting to use pin 5 (input B) of the SN74121D as a trigger source, and have connected a 2kohm resistor from pin 5 to ground to pull the pin low.
However, I am still measuring a voltage of 1.55V at pin 5.
Since the SN74121D requires a voltage level below 0.8V to be considered a logic low, the voltage at pin 5 not be low enough to trigger the device.
Should I choose the lower pull low lower resistor?
If yes, what value is suitable? Or have any suggestions?
Thanks!