This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC2G125: Ioff feature protecting the logic gates from being powered through IO pins when unpowered?

Expert 4525 points
Part Number: SN74LVC2G125
Other Parts Discussed in Thread: SN74LVC2G08,

Hi TI Logic Team,

Just wanted to double check, when the ICs are unpowered, the Ioff feature of eg SN74LVC2G125 and SN74LVC2G08 will prevent the parts to unintentionally be powered from an signal present at the the input pins, correct?
Is there anything to account for (eg pull-up/down on the OE pins)?

Thanks a lot & Best Regards,
KF