Hi,
We are using SN74LVC1G08DCKR AND gate in our design. Our products are installed in customer premises. Suddenly one product stopped working and when we checked it, we have found that the AND gate input (PIN 2) is always low even though there is a 10K pull-up t0 3.3V. And in PIN 2, there is no other signals except the pull up resistor. Can you please tell me whether any problem happened to the AND gate? Is the GATE damaged? Please give your feedback ASAP. I have a detailed picture which explains the issue more clear. If you need it I can send it to you.
BR Muthu