Part Number: SN74HCS245-Q1
Hi Team, seeking for some support.
Looking for the differential mode and common mode input impedance for SN74HCS245-Q1 (Schmidtt Trigger)
Thank you.
-Mark
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74HCS245-Q1
Hi Team, seeking for some support.
Looking for the differential mode and common mode input impedance for SN74HCS245-Q1 (Schmidtt Trigger)
Thank you.
-Mark
For practical purposes, approximately inifite. If you really want to compute a value, see [FAQ] What is the impedance of the device's input pin?
Hi Clemens,
The input capacitance and resistance are in parallel. And they are so small/large that you usually ignore them.
The input leakage current is at most 1 µA; the resulting power dissipation is not noticeable.
Hey Mark,
If you're looking for a model of the device - we have an IBIS model that includes the input impedance on our website.
https://www.ti.com/product/SN74HCS245-Q1?dcmp=dsproject&hqs=#design-tools-simulation
We also have SPICE models for many HCS family devices that have the input / output impedance. This particular one doesn't have a model, but I pulled up the appropriate part of the SPICE model from another device in the family that might help you out:
.PARAM RA = 240000000
.PARAM RB = 240000000
.PARAM CA = 1e-11
.PARAM CB = 1e-11
RA A GND {RA}
RB B GND {RB}
CA A GND {CA}
CB B GND {CB}Hi Emrys,
Seeking further support for the customer.
1.) Can you send me the full spice model netlist for other HCS circuits below including the .SUBCKT line and ENDS? The spice netlist below is missing some information.
Sure - there are many available on TI.com -- one example is here: https://www.ti.com/product/SN74HCS125#design-tools-simulation
2.) Can you please send me the max power dissipation (both peak and average at the input pins for the part. I need to compare it with power dissipated from ESD pulses.
No, that's not something we specify. You can find the ESD ratings of the device in the datasheet.