This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LXC2T45-Q1: SN74LVC vs. SN74LXC

Part Number: SN74LXC2T45-Q1


Hello Team, who can explain what the different is between the two families?

Especially 

SN74LVC2T45QDCURQ1

SN74LXC2T45QDCURQ1

Many Thanks

Josef

  • Hello Josef,

    The main differences between the two is the LXC family has:

    • Integrated pulldowns
    • Schmitt-Trigger inputs to tolerate slow or noisy input signals
    • A lower Vcc min; 1.1V vs 1.65V
    • Glitch-free power supply sequencing.
      • The power supplies can be powered (on/off) in any order without producing a glitch on the I/Os

    Regards,

    Josh