Part Number: SN74LVC1T45
Hi Experts,
I have two questions about SN74LVC1T45 power-up sequence.
Q1.
The SN74LVC1T45 PCN adds the following new power-up sequence recommendations: Does the SN74LVC1T45 manufactured before PCN require the same power sequence or does it apply only to products after PCN?
===============================
The recommendation is to first power-up the input
supply rail to help avoid internal floating while the output supply rail ramps up.
can be ramped up simultaneously.
===============================
Q2.
SN74LVC1T45-Q1 is a product with the same function as SN74LVC1T45.
The power sequence of this product is as follows.
I think the two products have the same basic design, but there is a difference in the power sequence. Which power sequence is recommended for SN74LVC1T45?
===============================
A proper power-up sequence is advisable as listed in the following:
1. Connect ground before any supply voltage is applied.
2. Power up VCCB.
3. VCCA can be ramped up along with VCCB.
TI recommends that the inputs are grounded during power up. Take care to assure that any state changes do not
affect system level operation.
===============================
Thanks in advance
Regards,
Toshi