Part Number: SN74ABT2245
Other Parts Discussed in Thread: SN74ABTR2245, SN74ABT245B
Hi Team,
We would like to ask your help regarding our customer's inquiry below.
Looking at the differences between SN74ABT2245 and SN74ABT245, I see the the drive strength (IOH / IOL) of the 2245 is considerable lower than that of the 245. Are the parts essentially identical with the exception of the 25 ohm resistors in the 2245 and is the existence of the resistors the reason for the lower current? If I were to use the 245 with external 25 ohm resistors, would I effectively accomplish the same circuit as the 2245 and achieve the same output current?
Regards,
Danilo