This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G07: Slew rate of output signal

Part Number: SN74LVC1G07
Other Parts Discussed in Thread: SN74LVC1G34

Hi, Logic team

I would like to know the slew rate of output signal from the characteristics in the datasheet. Because the post-stage circuit has a slew rate specification for the input signal.

The actual required specification is 50mV/ns during Vcc*30% and Vcc*70% as Vcc=1.8V. 

Could you give your comments if SN74LVC1G07 is satisfied the above specification? If not satisfied, please inform me about your recommended device .

Regards,

Tamio