Part Number: SN7407
I am using the SN7407N IC to send a square wave signal through. On a scope, I can see the signal getting to the input of the buffer but the output of the buffer is non-existent (no output). I am using 2 of the 6 buffers on this IC. For the unused buffers I have tied the buffer inputs to ground per the datasheet. I am using 10K pull-ups to 5V supply for the buffer outputs. I am trying to understand why I see no output on both of the actively used 2 buffers. What am I doing wrong? Please see my schematic attached. Thanks!