This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSF0102: What happens if VCCA is open?

Part Number: LSF0102


Hello,

If I have VCCB = 3.3V and VCCA is open, what voltage should be expected at VCCA? Is it left floating if its voltage is greater than VCCB - Vth?

Also, if VCCA is shorted to ground, how much current flows into VCCA? Is it approximately VCCB/200kOhm (ignoring the relatively small ON resistance of the FET)?

Thank you!

Best regards,

Zach Kimble

  • Hi Zach,

    If I have VCCB = 3.3V and VCCA is open, what voltage should be expected at VCCA? Is it left floating if its voltage is greater than VCCB - Vth?

    Note that we will not be able to guarantee its' operation as this is not a recommended condition. However, Vref_B is connected internally to the gate and drain of internal MOSFET. Hence, yes; when the transistor is turned on, the vref_A is pulled to Vref_B - Vt.

    Also, if VCCA is shorted to ground, how much current flows into VCCA? Is it approximately VCCB/200kOhm (ignoring the relatively small ON resistance of the FET)?

    Also yes, as with Vth accounted for it's typically (Vref_B-Vref_A-Vth) /200K. 

    Best Regards,

    Michael.

  • Thank you Michael! I have no further questions at this time.