Dear sirs,
I have question about this description in document "SCES877A – DECEMBER 2018 – REVISED JULY 2020".
-----
8.3.9 Supports High-Speed Translation
The SN74AXC4T245 device can support high data-rate applications. The translated signal data rate can be up
to 380 Mbps when the signal is translated from 1.8 V to 3.3 V.
-----
How do I calcurate the data-rate.
In chapter 6.11, tpd is less than 6ns when VCCA=1.8V and VCCB=3.3V.
There are no description output slew rate specs.
How is 380Mbps derived by above specs?
Best regards,