This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G97-Q1: V_I rating relationship with VCC

Part Number: SN74LVC1G97-Q1


Hello,

SN74LVC1G97-Q1 can be used with supply voltages between 1.65 and 5.5V and the input voltage rating specifies that the abs max is 6.5V. If the device VCC is powered at 3.3V (to be compatible with 3.3V logic), are the pins still 5V-tolerant? I understand that the input thresholds are related to VCC, but I want to confirm that the input voltage rating is not.

Thanks,

Nicole