Other Parts Discussed in Thread: SN74LVC07A
I am using this decoder chip in my design. This design requires the decoder to be powered down while the outputs are connected to CS pins of battery powered chips that stay powered on. These pins are externally pulled-up with 4.7k resistors to 3.3V power. I was having some trouble getting the chip to work the way I wanted to. The pull-ups were backfeeding through to the Vcc pin and preventing the outputs to go into high-Z mode when the chip lost power. I ended up connecting the Vcc pin to a really strong pull-down to get it to go into high-Z mode.
Looking for an alternative way to connect the chip, I found that the chip works like an open-drain device when I leave the Vcc pin floating. It seems to work exactly how I'd like it to. I'm nervous though because this doesn't seem like defined behavior that is spelled out in the datasheet. Are there any big issues I could run into using the decoder in this way?