This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0106: 5V signal (essentially from USB) to enable the level shifter

Part Number: TXB0106

Hi Experts,

I need your expertise for confirmation. Quick question about using TXB0106:

Say I use 3.3V for Vccb and 1.2V for Vcca, but I provide a 5V signal (essentially from USB) to enable the level shifter.
Is that a valid case?

I’m asking to be sure the max 5.5V shown in the datasheet means unrelated to Vccb or Vcca supplies.

My only concern is that OE is above both supplies. It's 5V while VCCA and VCCB are 1.2V & 3.3V.
Thank you in advance for your support.
Best regards,
Jonathan