This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV04A: Performance difference between SN74LV04A and SN74LVC04A

Guru 14780 points

Part Number: SN74LV04A
Other Parts Discussed in Thread: SN74LVC04A

Hi, 

Q1.
I am currently considering using the SN74LV04A (LV-A). There is a similar model number SN74LVC04A (LVC). Could you tell me the difference in specs between these two model numbers?

Q2.
I plan to use it under the conditions of a power supply voltage of 3.3V and an input voltage of 5.0V. Does the SN74LV04A have a tolerant function?

Thanks,

Conor