This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AUP1G99: Logic High Threshold

Part Number: SN74AUP1G99


Hi, I have a question about SN74AUP1G99 input High threshold. The chip in our application is supplied by 3.3V voltage, and the input A/B/C/D are connected to 2.5V through a 5K pull-up resistor. Will SN74AUP1G99 treat 2.5V as logic high when the inputs are not pulled down by the other circuits? From the date sheet, it should be treated as logic HIGH at Vcc = 3V. Just try to confirm it still applies to Vcc = 3.3V.